CAP#.T

Description

This will return the captured local clock time. This value is always captured in addition to the position selected by CAP#.SOURCE. The drive local time is the time since boot is in nanoseconds.

Examples

Code

-->CAP1.T
0 [ns]
-->

Context

For more information please refer to Capture.

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read Only
Units nanoseconds
Range

N/A

Default Value N/A
Data Type Unsigned64
See Also CAP#.SOURCE, CAP#.P
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.